SCADA & MES Global Support
CitectTM SCADA Compatibility Matrix

 

For your easy reference, this matrix describes the compatibility of Citect SCADA with various versions of Microsoft® Windows® operating systems.

Supported Supported
Not Supported Not Supported
Not confirmed at this time Not confirmed at this time
Citect SCADA
2016 2015 7.40 7.30 7.20 7.10
Operating System
Windows® Server 2016 Supported(Note5) Not confirmed at this time Not confirmed at this time Not Supported Not confirmed at this time Not Supported
Windows 10 Supported Supported(Note4) Not confirmed at this time Not confirmed at this time Not confirmed at this time Not Supported
Windows Server 2012 R2 Supported Supported Not confirmed at this time Not confirmed at this time Supported(Note2) Not Supported
Windows 8.1 Supported Supported Not confirmed at this time Supported(Note3) Supported(Note2) Not Supported
Windows Server 2012 Supported Supported Supported Supported(Note3) Supported(Note2) Not Supported
Windows 8 Supported Supported Supported Supported Supported(Note2) Not Supported
Windows Server 2008 R2 Supported Supported Supported Supported Supported Not confirmed at this time
Windows 7 Supported Supported Supported Supported Supported Supported(Note1)
Windows Server 2008 Not Supported Not Supported Supported Supported Supported Supported
Windows Vista Not Supported Not Supported Supported Supported Supported Supported

NOTE 1 – Requires CitectSCADA 7.10 Service Pack 3 installed for Windows 7 compatibility

NOTE 2 – Requires CitectSCADA 7.20 Service Pack 5 installed for Windows 8.1 & Windows Server 2012 R2 compatibility

NOTE 3 – Requires CitectSCADA 7.30 Service Pack 1 installed for Windows 8 and Windows Server 2012 compatibility

NOTE 4 – Requires CitectSCADA 2015 Service Pack 1 installed for Windows 10 compatibility

N.B. In November 2016, the CitectSCADA and StruxureWare SCADA Expert Vijeo Citect product suites were consolidated under our Citect SCADA brand. For more information,please refer to the Citect SCADA 2016 FAQs document on the SCADA & MES Support Website.