Go Back   Forums > Groups / Lists (Archived Content) > UsersList (Closed)

You are NOT logged in. Please clear cookies from the domain .citect.schneider-electric.com and login.

 
 
Thread Tools Display Modes
  #1  
Old October 2nd, 2003, 01:54 PM
Archived Message
Guest
 
Posts: n/a
Default Siemens PRU Communication with PROFIBUS

Im trying to communicate with a SIEMENS PRU 10.64 with the Profibus card CP5512 in the pc.
We know that its working in Desigo Insight but we want to use it in standard citect, has anyone tried this?
what is the correct setup?
thanks in advance.
Patrick Hoeve
Bouwhuis-RegeltechniekThe Netherlands
PatrickHoeve@bouwhuis-regeltechniek.nl
__________________
  #2  
Old October 3rd, 2003, 01:09 PM
Archived Message
Guest
 
Posts: n/a
Default RE: Siemens PRU Communication with PROFIBUS

Hi!
We once installed a Citect 5.21 with a profibus card from Softing (Profiboard PB-IF-03), and if I remember right, we had 3 PRU2.64 on the Profibus network.
We had 2 major problems;
Getting the right profibus-driver in Citect.
Getting the communication-profile for the PRUs. (Not even the Profibus Guru of Landis&Staefa in Sweden was sure which profil to use).
But now the system has been running for several years.
Urban Larsson
AutomatikSystem AB
urban@automatiksystem.se

-----Original Message-----
CP5512 in the pc.
We know that its working in Desigo Insight but we want to use it in standard citect, has anyone tried this?
what is the correct setup?
thanks in advance.
Patrick Hoeve
Bouwhuis-RegeltechniekThe Netherlands
PatrickHoeve@bouwhuis-regeltechniek.nl
__________________
  #3  
Old October 15th, 2003, 07:16 AM
Archived Message
Guest
 
Posts: n/a
Default AW: Siemens PRU Communication with PROFIBUS

Hi Urban
Can you provide me with more Information on that? We are also trying to talk to a PRU1.64 and we are interested in the Setups for the communication.
Kind regards
Daniel
Novitas Elektronik AG
user@novitas.ch

-----Ursprüngliche Nachricht-----
Gesendet: Freitag, 3. Oktober 2003 14:03
An: Citect Users Email List
Betreff: RE: Siemens PRU Communication with PROFIBUS

Hi!
We once installed a Citect 5.21 with a profibus card from Softing (Profiboard PB-IF-03), and if I remember right, we had 3 PRU2.64 on the Profibus network.
We had 2 major problems;
Getting the right profibus-driver in Citect.
Getting the communication-profile for the PRUs. (Not even the Profibus Guru of Landis&Staefa in Sweden was sure which profil to use).
But now the system has been running for several years.
Urban Larsson
AutomatikSystem AB
urban@automatiksystem.se
-----Original Message-----
CP5512 in the pc.
We know that its working in Desigo Insight but we want to use it in standard citect, has anyone tried this?
what is the correct setup?
thanks in advance.
Patrick Hoeve
Bouwhuis-RegeltechniekThe Netherlands
PatrickHoeve@bouwhuis-regeltechniek.nl
__________________
  #4  
Old October 21st, 2003, 01:40 PM
Archived Message
Guest
 
Posts: n/a
Default RE: Siemens PRU Communication with PROFIBUS

Hi!
Heres the profibus partion of the citect.ini used to talk to PRU2.64 urban@automatiksystem.se

!----- Landis & Staefa UNIGYR -----
[ProfiBD]
! polltime=30
debugstr=* all
window=0 ! Trace Window - 1=on; 0=off
log=0
!
! Bus Parameters
!
Local_Address=32
Local_Segment=255
!
!medium_red=0
tsl=744
min_TSDR=95
max_TSDR=140
tqui=2
tset=160
ttr=93750
g=1
in_ring_desired=255
hsa=32
max_retry_limit=1
!
! CRL Header
!
nr_of_entries=1
poll_sap=32
!symbol_length=20
ass_abt_ci=4096
!vfd_pointer_supported=0
[PRU]
MaxOutStanding=1
!TestIndex=9306
!
! CRL Entry
!
conn_type=MMAC
conn_attr=0
!lli_sap=0
!multiplier=1
!
max_scc=2
max_rcc=2
max_sac=2
max_rac=2
!
ci=60000
!
max_pdu_snd_high=220
max_pdu_snd_low=220
max_pdu_rcv_high=220
max_pdu_rcv_low=220
!
feature_support_0=24 ! 24
feature_support_1=48 ! 48
feature_support_2=128 ! 128
feature_support_3=88 ! 88
feature_support_4=48 ! 48
feature_support_5=216 ! 216
!
!symbol=
!vfd_pointer=0
!extension=0
!

Urban Larsson
AutomatikSystem AB

> -----Original Message-----
>
> Hi Urban
> Can you provide me with more Information on that? We are also trying
> to talk
>
> to a PRU1.64 and we are interested in the Setups for the communication.
> Kind regards
> Daniel
> Novitas Elektronik AG
> user@novitas.ch
>
> -----Ursprüngliche Nachricht-----
> Gesendet: Freitag, 3. Oktober 2003 14:03
> An: Citect Users Email List
> Betreff: RE: Siemens PRU Communication with PROFIBUS
>
> Hi!
> We once installed a Citect 5.21 with a profibus card from Softing
> (Profiboard PB-IF-03), and if I remember right, we had 3 PRU2.64 on
> the Profibus network.
> We had 2 major problems;
> Getting the right profibus-driver in Citect.
> Getting the communication-profile for the PRUs. (Not even the
> Profibus Guru of Landis&Staefa in Sweden was sure which profil to use).
> But now the system has been running for several years.
> Urban Larsson
> AutomatikSystem AB
> urban@automatiksystem.se
> -----Original Message-----
> communicate with a SIEMENS PRU 10.64 with the Profibus card
> CP5512 in the pc.
> We know that its working in Desigo Insight but we want to use it in
> standard citect, has anyone tried this?
> what is the correct setup?
> thanks in advance.
> Patrick Hoeve
> Bouwhuis-RegeltechniekThe Netherlands>
> PatrickHoeve@bouwhuis-regeltechniek.nl
__________________
 

Thread Tools
Display Modes

Posting Rules
You may not post new threads
You may not post replies
You may not post attachments
You may not edit your posts

BB code is On
Smilies are On
[IMG] code is On
HTML code is Off

Forum Jump

All times are GMT +11. The time now is 04:54 PM.
© Schneider Electric (Australia) Pty Ltd, 2013